The configuration of the input action defines how a visualization user specifies a value and to which variable the value is written.
|
“Input type” How the input is prompted |
|
|
“Default” |
Input field, or if necessary a virtual keyboard (if the display variant does not have a physical keyboard) Note: The default option for text input at runtime is set in the Visualization Manager: “Dialog Settings” tab, “Settings for Default Text Input”. |
|
“Text input” |
An input field is displayed. As the visualization user, you can use the keyboard to specify a number or a text. Requirement: The display variant has a keyboard as input device. |
|
“Text input with limits” |
An input field is displayed. You use the keyboard to specify a number or a text. The field also shows the value range for the input. When a limit is passed, the input value is displayed in red. Requirement: The display variant has a keyboard as input device. |
|
“VisuDialogs.Keypad” |
A virtual keyboard opens. You use it to specify a number or a text. |
|
“VisuDialogs.Numpad” |
A virtual keyboard opens. You use it to specify a number. |
|
“VisuDialogs.NumpadExtended” |
A virtual keyboard opens. You use it to specify a number. Hexadecimal and exponential notation are also permitted here. |
|
“Choose variable to edit” |
|
|
“Use text output variable” |
|
|
“Use another variable” |
Example: |
|
“Initial display format” |
Placeholder with format definition. It defines the output format for the variable value and the input limits. Example: |
|
“Min” |
Minimum value of the input limit. If a user specifies a lesser value, then it is not accepted.
|
|
“Max” |
Maximum value of the input limit. If a user specifies a greater value, then it is not accepted.
|
|
“Dialog title” |
Text displayed in the title bar of the dialog. Optional.
|
|
“Password field” |
|
|
“Position to Open Input Dialog” |
Initial position for the opening input dialog relative to the calling visualization |
|
“Use global setting (from the Visualization Manager)” |
Requirement: This option is available only when displaying on a TargetVisu or as a WebVisu.
|
|
“Centered” |
|
|
“Position” |
Note: Use the corresponding input options for specifying the position in the X-direction and the Y-direction. |
|
“X” |
Horizontal X-position for the upper left corner of the opening dialog Input options:
|
|
“Y” |
Vertical Y-position for the upper left corner of the opening dialog Input options:
|
: The input value is written to the text output variable of the element. This is the
variable that is assigned in the
: